{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does Vijeo Designer support FTPs (File Transfer Protocol Secure)?
The Latest versions of Vijeo Designer include new features to be compliant with the Cybersecurity.
The goal of this article is to inform about FTPs (File Transfer Protocol Secure) support from the version VJD 6.2 SP12.

This article is applicable to the following products:
Harmony P6, HMIGTU, HMIGTO, HMISTU, iPC, XBTGT,

This topic is related to Vijeo Designer

From Vijeo-Designer V6.2 SP12, FTPs (File Transfer Protocol Secure) has been implemented to replace FTP for Downloading, uploading and transferring data. FTPs encrypts data transmitted over network to protect the data against sniffing.
FTPs operation follows the same procedure as FTP, there are no extra and special configuration required.

Schneider Electric Global

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: