{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
EcoStruxure Power Operation (EPO) 2021: No option to configure OPC UA Client (v3.04.06.000) in Configurator tool
Issue
After installing supplied OPCUA Client driver along with EPO2021 ISO, unable to configure OPCUA Client in Configurator since it doesn’t have option.

Environment
EcoStruxure Power Operation (EPO) 2021

Cause
Known issue with the default provided OPCUA v3.04.06.000 driver along with EPO2021 ISO.

Resolution
Download the latest available OPCUA driver (currently v4.01.04.000 is available) from the AVEVA support site and install it.
If in case you don't have access to AVEVA site, then contact SE Tech support team.