{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the OPCUA client function block in Control Expert access the OPCUA server module BMENUA0100 via the backplane port?
Issue:
OPCUA client function block in Control Expert accessing the OPCUA server module BMENUA0100 via the backplane port


Product Line:
EcoStruxure Control Expert


Resolution:
No. The OPCUA client function block can access the UA server only by the external port of the BMENUA0100 module or the embedded Ethernet port of the CPU