Issue:
REAL data type variables data not showing correctly in Vijeo Designer when communicating to a Unity Quantum PLC
Product Line:
Vijeo Designer, Quantum PLC
Resolution:
The REAL data type variables may not show correctly due to word order not set correctly in Vijeo Designer. When the HMI is communicating to an Unity Quantum PLC the double word order must be "High word first". To change the word order, expand the I/O manager in the navigator and double click on the equipment.
Next, ensure that the Double Word word order is set to "High word first"
Released for:Schneider Electric Global