{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why "OFSLog" shows the message “Not enough space”?
Some customers observe that the memory space consumed by OFS grows regularly.
At the end, "OFS" doesn't work anymore.  
Customer have to restart the PC to make "OFS" operational again.

print screen

Explanation:
there's a memory fragmentation which has the same effects as a memory leak.
This effect is due to the garbage collector which is active by default and must be deactivated.
On OFS V3.63 SP2, it will be disabled by default and not enabled.

To deactivate the garbage collector, you must therefore:
• stop OFS
• edit C:\ProgramData\Schneider Electric\OFS\3.63.0.0\ofsinternal.xml
• replace <add value="true" key="GarbageCollector"/> by <add value="false" key="GarbageCollector"/>

In the OFS log, we must have Garbage collector is not active

Schneider Electric Global

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: