{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to manually check and correct Auxiliaries from older project which are not compatible due to new offer Auxiliary Acti9 and Multi9 evolution in V2.5.XX in EcoStruxure PowerBuild – Rapsody.
Issue: Check and correct the non-compatible auxiliaries from project created in version older than V2.1.x.

Product Line: EcoStruxure Power Build – Rapsody

Resolution:
With the new version V2.5.X of EcoStruxure PowerBuild- Rapsody, as the Auxiliaries Acti9 and Multi9 have evolved, it will cause a compatibility breach in EcoStruxure Power Build Rapsody when working on new version V2.5.X with project created in older version V2.1.X which had OF-SD selected for the following offers:
C120
iC60
iC60 double terminals
Acti9 C60H-DC
iSW NA
iDPN N Vigi
iDPN H Vigi
iDPN N Vigi G type

ACTI9 iC40
ACTI9 iCV40 Feeder
ACTI9 iID40
ACTI9 iIG40
ACTI9 iDT40
ACTI9 iDD40 Head of group
ACTI9 iDD40 Feeder














Step1:
Open the old project SSD file in version V2.5.X by using the option “Open an Existing Project” or “Open a recent Project”.

Step2:
When pop-up for project update appears, choose “No”.


Step3:
From “Electrical Organization” tab, Generate functional Names as shown in below screenshot.




Step4:
Click on Update project button image.png and run the project update and check the box for option “Show only the modified references” to get the list of devices impacted.




Step5:
Export the list or save the screenshot for each impacted switchboard.


Step6:
Go to Product Choice and right click on the impacted devices and choose “Modify” and select the required characteristics.  Modify the impacted devices for all the switchboard.



Note: For project with more number of switchboard and devices with auxiliaries, it may take longer time to validate the devices.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.