Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

		
Search FAQs
DCE shows duplicate cameras for a single NetBotz 750/755 attached camera
Issue:
DCE shows duplicate cameras for a single NetBotz 750/755

Product Line:
Data Center Expert
NetBotz

Environment:
DCE (any version)
NBRK0750
NBWL0755
NBPD0165

Cause:
If you Remove a NetBotz 750 or 755 from DCE and that appliance had a connected camera, the camera will not get deleted from DCE surveillance.
The camera will appear as disconnected and show a test pattern. Re-adding the appliance even with the same camera re-adds the camera with a separate internal ID so DCE won't associate it with the newly added NetBotz.

Resolution:
After removing a NetBotz 750 or 755 with a connected camera from DCE, it is recommended that you delete the camera from the surveillance view in DCE.
If you do not, after you re-add the NetBotz even with the same camera, that camera will show as a duplicate and only one camera will actually capure clips going forward.

You should still be able to delete the camera after re-adding the appliance as you will see one communicating and one not communicating. Delete the non-communicating camera.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Careers
  • Sustainability
  • Electricity 4.0
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings