Issue:
An error message gets displayed at the bottom, stating: "The following user font is missing. Font font name."
Product Line:
Vijeo Designer, HMIG3U.
Resolution:
It sometimes happens, when compiling a project, that one or more fonts are omitted from the compiled file, which causes the error message. We don't know exactly why this is happening.
To fix this, he suggests trying to do a "Build - Clean All" and then do a "Build - Build All" again. Normally, the recompiled file is corrected and includes the required font(s).
Released for:Schneider Electric Global