{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Where can I find the detailed description of some safety functions blocs used in machinery applications and available in the safety libset of Control-Expert ?
Question :
Where can I find the detailed description of safety machinery functions blocs listed below and available in the safety libset of Control-Expert ?
  • Folder “ActuatorConnection” :
    • S_EDM
    • S_ENABLE_SWITCH
    • S_ESPE
    • S_GUARD_LOCKING
    • S_GUARD_MONITORING
    • S_MODE_SELECTOR
    • S_OUTCONTROL
  • Folder “Muting” :
    • S_MUTING_PAR
    • S_MUTING_SEQ
  • Folder “SensorConnection” :
    • S_ANTIVALENT
    • S_EQUIVALENT
    • S_EMERGENCY_STOP
    • S_TWO_HAND_CONTROL_TYPE_II
    • S_TWO_HAND_CONTROL_TYPE_III
Answer :

Overall description is available in user documentation available in Control-Expert. However, further details (complete state machine and detailed transitions)  are available in the standard from PLCopen.org website and attached to this FAQ: “plcopen_safety_part_1_v1.0.pdf”.

Note: these function blocs are not following the further revisions of this specification from PLCopen (example: “PLCopen Safety Part 1 version 2.01”). They have been coded on the basis of version V1.0 of the PLCopen standard.

Schneider Electric Global

Attachment(s)
plcopen_safety_part_1_v1.0.pdf [1.36 MB]