Issue:
Why can't I access all the parameters on the ATS480 soft start?
Product Line:
ATS480
Environment:
Menu access
Cause:
n/a
Resolution:
First go to Menu 10: My Preferences, then select Parameter access.
The ATS480 offers 3 levels of Access: Basic, Standard and Expert
Basic gives you access to these menus: Simply Start, Monitoring, Input/Output, Display, Diagnostics and Device Management
Standard gives you access to ALL menus, but some parameters are still not visible
Expert gives you access to all menus and all parameters.
Released for:Schneider Electric Global