What is the maximum number of TCP/IP connections for the BMEP586040S
The maximum number of simultaneous TCP/IP connections on the BMEP586040S is the same as on the BMEP586040. The following table shows the maximum number of connections for the M580 CPU's.
Released for:Schneider Electric Global
Explore more
Product:
BMEP586040S
Articles that might be helpful
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.