Issue:
Would like to utilize the Dell VxRail feature in PowerChute Network Shutdown.
Product:
PowerChute Network Shutdown version 4.5 & 5.x
Environment:
Dell VxRail and VMware ESXi
Cause:
Informational
Solution:
Dell VxRail is only supported with Network Management Card 3 (AP9640, AP9641) in a
Smart-UPS with firmware (SU) v2.2 and above on the NMC 3.
Smart-UPS Ultra with firmware 2.5.1 and above on NMC 3.
Symmetra LX with firmware 2.5.0.3 and above on the NMC 3.
Symmetra PX, PX2 with firmware 2.4 and above on the NMC 3.
Galaxy VS with Firmware v6.101+.
Galaxy VL with Firmware v14.4+.
Galaxy VXL with firmware v11.31+.
Examples of supported Smart-UPSs: SMT, SMTL, SMX, and SRT model UPSs with AP9640 or AP9641 running firmware SU 2.2 or above.
NOTE: Currently not supported with Easy UPS.
Released for:Schneider Electric Global