{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you import the .eds library file into Control Expert?

Issue

Import .eds library

Product Line

Modicon M580

Modicon M340

Modicon Quantum

Environment

EcoStruxure Control Expert

Resolution

Having the ability to have a company or multiple people working on the same project standardize on an .eds library will save time and frustration. To do this you can import a full .eds library into Control Expert. Here are the steps to import the library:

1. Open a Control Expert project.

2. Open the DTM browser

3. Right click on a module, select Device Menu, Additional functions, and Import EDS library.

4. Navigate to where the the exported file is saved.

5. Wait for the import to be successful