{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does the M340 Can-Open master detects the presence of the devices which are not configured?
The answer is yes:
This behavior is part of the bootup procedure specified in the standard "CiA302".
At the end of the bootup procedure, after all expected slaves have got their configuration data, a "start all nodes" command is sent by the master.
So each devices connected to the network are identified.

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: