{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the ideal lubricant fill quantity for the Lexium™ MC12 carrier (LXMMC12CA51S100)?
A Lexium™ MC12 carrier has four lubrication nipples (1–4) to fill the two lubrication reservoirs. The upper lubrication reservoir (5) is filled by lubrication nipple 1 or 2, the lower lubrication reservoir (6) is filled by lubrication nipple 3 or 4.

LXMMC12CA51S100

The ideal lubricant fill for each Lexium™ MC12 carrier reservoir is 0.65g per fill.
Details of recommended lubricants can be found in the Lexium™ MC12 Multi-Carrier Hardware Guide.