1- Issue:
Control Expert v15.3 crash when displaying on Ultra Wide screen resolution 5120 x 1440.
2- Product Line
Control Expert v15.3
3- Environment:
Windows 10
4- Resolution:
The maximum supported resolution for Control Expert v15.3 is 2560 x 1440 with Scale and Layout at 125%.
The resolution 5120 x 1440 will be supported in Control Expert v16.0
Control Expert v15.3 crash when displaying on Ultra Wide screen resolution 5120 x 1440.
2- Product Line
Control Expert v15.3
3- Environment:
Windows 10
4- Resolution:
The maximum supported resolution for Control Expert v15.3 is 2560 x 1440 with Scale and Layout at 125%.
The resolution 5120 x 1440 will be supported in Control Expert v16.0
Released for:Schneider Electric Global