{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why can't SSOLR be used with M10 factory form (Marine certification) in Motor Starters?
Issue:
Solid state overload relays are not available for marine certification

Product Line:
9065SF Overload Relays - GIC Product

Environment:
US Product

Cause:
Certification

Resolution:

For the SSOLR  there are two reasons that left this component off of the testing and certification process:

1) part of the marine requirement is that ALL current carrying parts are COPPER. The control circuit component of the MotorLogic that is supplied with the product is not and therefore would not meet the criteria.

2) Since it would require a redesign of the above component it has since never been updated to include the SSOLR.

Schneider Electric Global

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: