AI-Powered microgrids: Optimizing the balance
- By Eric Fourboul, Jacques Kluska, Rémi Paccou, Gauthier Roussilhe
- 24 Nov 2025
- 5 min
New research across 11 operational sites reveals the conditions under which artificial intelligence delivers both cost savings and carbon reductions, and when it doesn't.
Artificial intelligence has entered the operational heart of distributed energy systems, promising to optimize everything from battery dispatch to grid exchanges in real time. The question is no longer whether AI can improve microgrid performance, but under what conditions that improvement serves both economic and environmental objectives.
Our latest study, "AI-Powered Microgrids", provides an empirical answer. Drawing on two years of operational data from 11 microgrids across Europe, North America, and Australia, the research distinguishes between what the physical infrastructure achieves on its own and what algorithmic intelligence adds. The findings challenge common assumptions about digital optimization and reveal a more nuanced picture: AI amplifies the logic of the systems it serves, for better or worse.
Before any AI enters the picture, a simple microgrid operating under basic self-consumption rules already delivers substantial environmental value. Across all 16 impact categories analyzed — from climate change and resource depletion to water use and toxicity — the heuristic baseline consistently outperformed grid-only operation. Local photovoltaic generation displaces carbon-intensive imports, battery storage smooths demand, and reduced transmission losses compound the effect.
This baseline matters because it establishes that environmental performance begins with infrastructure design, not digital sophistication. The microgrid's physical configuration — its capacity to generate, store, and manage energy locally — creates the foundation for decarbonization. Intelligence can refine that performance, but it cannot manufacture benefits that the system's architecture does not already enable.
When AI-based predictive control was introduced across the same infrastructure, it delivered exactly what it was designed to do: reduce costs. The algorithm, configured to minimize electricity expenses, achieved an 18 % cost reduction on average, roughly €200,000 in annual savings across the portfolio. Ten of the 11 sites recorded positive financial returns.
What the AI was not explicitly told to do was reduce carbon emissions. Yet in some contexts, it did precisely that. The South Australian facility, equipped with significant photovoltaic overcapacity and operating within a market where time-of-use tariffs correlate with grid carbon intensity, saw both a €124,500 reduction in costs and a 328-ton decrease in CO₂ emissions. Economic and environmental objectives converged because the market structure made them compatible.
In contrast, the California site achieved €27,533 in savings but increased emissions by 51 tons. Here, electricity prices reflected scarcity and volatility rather than carbon content. The AI responded rationally to the signals it received, importing cheaper power during periods of fossil-fueled baseload generation and exporting less during high-carbon peak hours. The algorithm optimized the objective it was given, but that objective was decoupled from climate impact.
The research identifies four structural factors that determine whether AI optimization aligns economic and environmental performance:
Grid carbon intensity and abatement potential
In low-carbon systems like France, where nuclear and hydro dominate, further emission reductions are marginal. AI-driven optimization yields limited environmental benefit because the baseline is already clean. Conversely, in carbon-intensive grids, the potential for substitution is greater if the right incentives exist.
Price-carbon correlation
When electricity tariffs reflect real-time carbon intensity, cost minimization naturally drives decarbonization. Where they diverge, optimization follows price signals that may favor fossil generation during low-cost periods.
Control logic and self-consumption displacement
Rule-based heuristics prioritize local renewable use. AI, focused on cost, may substitute on-site solar with cheaper grid imports, eroding the implicit environmental gains of simpler strategies.
Battery cycling and round-trip losses
Increased cycling under AI control raises total energy throughput. When the carbon differential between charge and discharge periods is small or inverted, efficiency losses translate directly into additional emissions.
These factors are not algorithmic flaws. They are design realities. AI does not autonomously pursue sustainability; it pursues the objectives embedded in its environment. Where those objectives align with climate goals, AI becomes a lever for coupled optimization. Where they do not, it remains a financial tool with neutral or adverse environmental effects.
The lesson from this research is systemic rather than technical. The environmental value of AI-powered microgrids depends less on the sophistication of the algorithm than on the coherence of the systems it operates within, including tariff structures, regulatory frameworks, grid composition, and infrastructure flexibility.
“Across the 11 sites, the evidence is unambiguous: algorithmic optimization mirrors the priorities it is given. When cost and carbon are structurally aligned, AI becomes an agent of decarbonization; when they diverge, it faithfully amplifies that separation.”– Jacques Kluska, Rémi Paccou
This insight has practical implications:
Policymakers
Embed carbon intensity in tariffs via dynamic or carbon-indexed pricing.
Microgrid operators
Assess whether baseline control already captures environmental gains before layering AI.
Technology providers
Align optimization objectives with sustainability outcomes rather than treating them as separate.
Future iterations of this work will explore carbon-aware optimization: control algorithms that explicitly balance cost and emissions rather than treating carbon as an incidental outcome. Early modeling suggests that hybrid objective functions can achieve substantial environmental improvements at marginal economic trade-offs, particularly in markets where price and carbon signals remain decoupled.
The research also points toward a broader agenda: the development of AI systems that integrate real-time carbon intensity data, physically grounded battery degradation models, and multi-criteria environmental indicators into their operational logic. These advances would shift intelligence from reactive optimization toward proactive stewardship — systems designed not merely to follow market signals, but to reshape energy flows in ways that serve long-term sustainability.
For now, the evidence is clear. Artificial intelligence can optimize microgrids for both profit and planet, but only when the conditions for convergence exist.
Explore the complete findings, data, and policy insights in the full AI-Powered Microgrids report from the Schneider Electric Sustainability Research Institute.
Latest from the Sustainability Research Institute
Time to power: A generational cycle of modernization in the US
Introducing the integrated Net Present Value framework
Original insights on the decarbonization potential of Brazil through innovation
Demand-pull policy framework for emission intensive industries