{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the part number for replacement internal red reset bar on the Class 8536 Type SF_ starter?
Issue:
Replacement Reset Bar on the Class 8536 Type SF_ starter

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8536 8736 Type SF, NEMA Contactors and Starter, Size 4

Resolution:
Replacement part number for the internal, red reset bar is 31075-008-01.  This piece snaps onto the overload reset mechanism.

Schneider Electric Global