Can you get an external keypad on a NEMA 3R E-FLEX drive?
Published date:
26 July 2019
Issue:
External keypad option for E-Flex Nema 3R drive
Product Line:
Altivar E-Flex drives
Environment:
NEMA 3R only E-Flex drives
Cause:
Needs to order an NEMA 3R -E-Flex drive with a remote keypad display mounted on the door.
Resolution:
The E-Flex drive is obsolete. External keypad was not available on the E-Flex. The replacement ATV660 drive also does not have an option for external keypad on Nema 3R as they are not UV protected.