Issue:
What is the part number for the cover or guard for XALK174?
Product Line:
Push Buttons and Operator Interface
Environment:
22 mm Harmony Control Stations
Cause:
Product Features
Answer:
There is no cover or guard available for the mushroom head push button. There is a raised area on the front of these XALK enclosures which will not allow
a guard the be mounted flush to the surface.
What is the part number for the cover or guard for XALK174?
Product Line:
Push Buttons and Operator Interface
Environment:
22 mm Harmony Control Stations
Cause:
Product Features
Answer:
There is no cover or guard available for the mushroom head push button. There is a raised area on the front of these XALK enclosures which will not allow
a guard the be mounted flush to the surface.
Released for:Schneider Electric Global