{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is it possible to use 3D label ZBY9*2* with XALD/XALK01 ?
The flat surface of the XALK01 is a rectangle 55,3 +/- 0,25 X 59,5 +/- 0,26
The 3D label ZBY9*2* is a circle diameter 60 +/- 0,2
So it could fit but not perfectly
Another option could be to select marked control station:
- Emergency stop        XALK01H29
- Arrêt d'urgence         XALK01HFR
- Not-Halt                    XALK01H44
Unfortunately, no other markings for control station

Schneider Electric Global