{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can ATS01N2...LU, QN, RT be started without external control wires?
Issue:
Start ATS01N2...LU, QN, RT without control wires.

Product Line:
Altistart 01 Soft Starters with "LU", "QN", or "RT" at the end of the part number

Environment:
All

Cause:
Need to start the Soft Starter with power up

Resolution:
Add a jumper between terminals LI+ and LI2.  This provides a continuous RUN command.  When power is supplied to the ATS01, it will immediately begin to start the motor.  Removing power will result in a freewheel stop.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Global