{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is Windows 7 compatible with SoMove, PowerSuite and PC Soft?

Issue:
Compability between Windows 7 and SoMove, PowerSuite and PC Soft.

Product Line:
SoMove, PowerSuite and PC Soft

Environment:
All versions

Cause:
None

Resolution:
SoMove is compatible with Windows 7, Windows 8 and 10.
PC Soft has been discontinued for many years and will not run under Windows 7.
Powersuite will work on Windows 7 if you have patch 3 installed.