{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the appropriate replacement for an ATV11 drive?
Issue:
Needs a replacement part number for an ATV11 drive.

Product Line:
Altivar 11

Environment:
All models and serial numbers

Cause:
Determine the replacement for an ATV11 drive.

Resolution:
The recommended replacement for the ATV11 is the ATV12.  Select the ATV12 based on the motor horsepower, rated motor voltage and supply voltage (single or three phase).

Schneider Electric Global