Yes. Using Windows explorer simply insert the PCMCIA into a laptop. Copy the appli folder to a temporary folder. Now this appli folder can be copied onto any PCMCIA card and when inserted into the XBTF will load the saved application. Care must be taken when removing the PCMCIA from the laptop. The socket MUST be turned off before removing the PCMCIA card because it could sustain damage if removed hot.
Released for:Schneider Electric Global