Touching the top left and then the bottom right, one after another, will open the configuration screen if the application has the feature enabled.
The easiest way is to create a switch on the panel that accesses it directly. Simply set "operation" to system and then choose "Configuration" as the option.
Released for:Schneider Electric Global