{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the serial cable to connect an XBTN200, XBTN400 and XBTR400 HMI to a Modicon M340?


The XBTZ9980 cable allow the communication between Modicon M340 PLC series through Modbus RJ45 port and the following HMI PRODUCTS: XBTN200, XBTN400 and XBTR400.


-Specifications:
cable
-Connectors
XBT side J1 : RJ45 Male 8 points
PLC side J2 : RJ45 Male 8 points

-Length
2.5m

-Temperature
Working temperature : -20°C to +70°C
Storage temperature : -40°C to +80°C

-Certification
CE certified and CSA UL508
Fireproofing rating : UL VW-1 for the cable
ROHS compliance