{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the Maximum number of variables that the Harmony/Magelis line of HMIs supported by Vijeo Designer will handle?

Issue
What is the Maximum number of variables that the Harmony/Magelis line of HMIs supported by Vijeo Designer will handle?

Product Line
Vijeo Designer
XBTGC, XBTGT, XBTGH, HMISTO5, XBTGK, XBTGTW
HMISTU, HMIGTO, HMIGTU, Vijeo Designer Runtime for Windows (iPCs, HMIBMx, HMIG5U22, Harmony P6, Generic PC)

Resolution
Number of variables per panel (limit)
Vijeo Designer Runtime for Windows: Maximum 2500 variables per panel
All other target types: Maximum 800 variables per panel.

Number of variables per target (limit)
Vijeo Designer Runtime for Windows: 12000 max.
XBTGC / XBTGT / XBTGH / HMIGTO / HMISTO / HMISTU / HMIG2U / HMIG3U Series: 8000 max.
XBTGK Series: 8000 max.

NOTE: For iPCs, if persistent variables such as alarm variables and data logging variables are used, a maximum of 8000 variables can be supported for each iPC target.

Number of variables you can share (recommended)
Vijeo Designer Runtime for Windows: 400
XBTGC / XBTGT / XBTGH / HMIGTO / HMISTO / HMISTU / HMIG2U / HMIG3U Series: 300
XBTGK Series: 300

NOTE: The Maximum Number of Shared Variables is the recommended maximum number of variables that is shared at any one time NOT the maximum number of Sharing-enabled (Read-only or Read/Write) variables. In other words, the number of variables that you set to Read-Only or Read/Write has no limits; only the number of variables that are accessed by other targets is limited. Performance may become an issue if you exceed the recommended maximum.

Schneider Electric Global