Issue
Restrictions of Vijeo Designer "Limited Edition" (Unregistered)
Product Line
Vijeo Designer
Resolution
The functions of the Limited Edition product are identical to those of the full product with the following restrictions:
It is possible to create and simulate an application for all supported HMI types (Magelis STO Monochrome, STU, XBTGT, XBTGK, XBTGH, XBTGTW, HMI GTW, HMIGTO, HMIGTU, Smart iPC, Compact iPC, Flex iPC, S-Box PC, Box PC, Panel PC, and Rack PC)
However, the application cannot be downloaded to a physical HMI except for Magelis STO5 and STU.
Simulation is only available using simulated PLCs (offline mode).
Note: The HMISTO, the Color screen, are programmed with the EcoStruxure Operator Terminal Expert software and not the Vijeo Designer software
Released for:Schneider Electric Global