{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the replacement for the Modbus Plus ISA adapter AM-SA85-000 (single channel)?

Issue

What is the replacement for the Modbus Plus ISA adapter AM-SA85-000 (single cable)?

Product Line

Modbus Plus

Environment

AM-SA85-000

Resolution

The Modbus Plus ISA-SA85 adapter (AM-SA85-000) has been replaced with the (AM-SA85-030). This is basically the same Modbus Plus single channel adapter card. Part number AM-SA85-000, which included just the adapter is no longer actively sold. We now sell part number AM-SA85-030 which is a kit that includes both the adapter (AM-SA85-000) along with the latest version of the Modbus Plus driver suite CD.