{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the type of CF card used by the Magelis XBTGT7340 ?
Issue
What type of CF card can be used by the Magelis XBTGT or XBTGK Series of HMI?

Product Line
Magelis XBTGT, XBTGK

Environment
Physical HMI

Resolution
For Data Storage of Logging, Alarm Logs, Recipes, etc, the XBTGT and XBTGK series of HMI uses TYPE-II CF cards with a maximum capacity of 16GB formatted as Fat 32.

Schneider Electric Global