Issue
The user cannot select the ION_Data archive from the Reporting Configuration Manager's drop down menu after upgrading ION_Data archives from a previous version to PME 7.2/PME8.0
Product Line
Power Monitoring Expert (PME) 7.2.x, 8.x
Cause
This will happen after an archived database from a pre-Power Monitoring Expert (PME) 7.2 system has been upgraded because the Value for the Schema gets incorrectly set to ION_Data, When you go to Reporting Configuration Manager to select your archived database, it will not show up in the list as a database to choose.
Resolution
Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*
First, open SQL Server Management Studio and connect to the PME instance.
Then, expand the archived database and expand the tables folder.
Next, right click on "dbo.Registry" table and select the "edit top 200 rows" option. (as shown in screen shot below)
Next, edit a field in the Registry table in your archived database( dbo.Registry table). After upgrading your archive in PME7.2, the Value for the Schema in the Registry table will say 'ION_Data'.
User will need to edit the Value from "ION_Data" to "ION_Data_Archive" as shown below. Once that is done, your archived database will show up in Reporting Configuration Manager and you will be able to use this database in Reports.
Released for:Schneider Electric Global