{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Which phase does an ION8600 and ION8800 meter choose to measure frequency on?

An ION8600 and ION8800 series meter chooses the phase at which to measure the frequency on in a pseudo random fashion, where it picks phase A more often then any other phase. Also, the phase selection is done in such a way to account for unattached phases, and skip them (in the case where one or two phases are wired).

Date Created: November 27, 2009
Last Revised: December 23, 2009
Public
Original Author: TO
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL200781 V1.0, Originally authored by MiNe on 12/23/2009, Last Edited by MiNe on 12/23/2009
Related ranges: ION8800, ION8600

Schneider Electric Global