Issue
User would like to know what happens when energy reading of the CM2000 increases beyond 999,999 MWh with respect to the front panel display
Product Line
CM2000
Environment
Front panel
Resolution
The front panel display will roll over from 999,999 MWh to 000,000 MWh.
If reading Wh from front panel you would need to note that a roll-over has taken place. Also note that the LED next to Mega stays lit after the roll-over has occurred.
Released for:Schneider Electric Global