{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Power Monitoring Expert and USB Modems

Issue
User does not have a Physical COM port on the machine running Power Monitoring Expert (PME) Software and would like to test their modem connection through a direct connection



Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
Physical Servers

Modems

Cause
It is not recommended to use a USB to Serial converter dongle for Modem connection directly to the PME server

Resolution
Two main options for connecting modems to a physical server without a COMM port.

1) Add an internal PCI card with serial ports example (http://www.comtrolstore.com/RocketPort_Express_PCIe_4_Port_s/413.htm)

2) USB to Serial converter such as http://www.digi.com/products/usb/edgeport#models

Schneider Electric Global