{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Do Schneider Electric drives connect to Allen Bradley Blue Hose protocol?
Issue:
Schneider Electric drives connecting to Allen Bradley Blue Hose protocol.

Product line:
Altivar, ATV61 ATV71, ATV312, ATV12

Environment:
All models, all serial numbers

Cause:
Need to connect to Blue Hose

Resolution:
The term 'Blue Hose' is typically used with Data Highway Plus (DH+) protocol. Schneider does not offer a direct connection to that protocol in drives. Customer can use a 3rd party solution such as Anybus HMS Gateway to convert the Protocol to CANopen or Ethernet etc.