Issue
Is it possible to download an application configured in Vijeo Designer Buildtime software to a Harmony (previously branded Magelis) HMISTU with Part Numbers HMIS5T, HMISTU655, HMISTU855 using a USB-A to USB Mini-B cable?
Product Line
Harmony or Magelis branded HMISTU Family
Environment
Physical Human Machine Interfaces
Resolution
Yes, the Vijeo Designer HMI application can be downloaded using a USB A to USB Mini-B cable.
The recommended Schneider Electric catalog number for that cable is BMXXCAUSBH018 (1.8m long) or BMXXCAUSBH045 (4.5m long)
It uses the XBTZG935 USB driver which is installed when Vijeo Designer Buildtime software is installed.
Released for:Schneider Electric Global