Issue:
What are the programming requirements when installing a load reactor, a motor choke, or output filter?
Product Line:
All Drives
Environment:
All
Cause:
Installation
Resolution:
No, there are no drive settings that have to be changed when using a load reactor.
It would be best to verify with manufacturer of the reactor if they have any limitations on the Switching Frequency or Carrier Frequency, but no changes are required for the drive.
Released for:Schneider Electric Global