Issue
When attempting to view tables in PME the page will display an error " Async_ExceptionOccurred ".
Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment
Power Monitoring Expert Web Applications
Cause
This error can occur when the memory maximum has not been set in the SQL server. SQL server will attempt to use all of the available RAM for the system. Checking on the RAM usage for the Server SQL is installed on will show 98-100% usage.
Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*
When attempting to view tables in PME the page will display an error " Async_ExceptionOccurred ".
Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment
Power Monitoring Expert Web Applications
Cause
This error can occur when the memory maximum has not been set in the SQL server. SQL server will attempt to use all of the available RAM for the system. Checking on the RAM usage for the Server SQL is installed on will show 98-100% usage.
Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*
- Note the amount of total RAM the the system has available
- On the SQL server: Right-click the icon called "Computer" located on the desktop or in the start menu and select "Properties"
- Note the Installed memory (RAM)
- Open SQL Server Management Studio, choose the instance where PME is located (typically ION or the default instance), and log in. You will either need a SQL account with edit permissions or a Windows account with SQL edit permissions.
- In the navigation panel right click the instance name and select Properties. If you have multiple instances connected, be sure to select the instance where PME databases are located.
- Select the Memory tab
- Set the maximum memory to roughly half of the available RAM for the system. Your individual requirements may vary.
- Click "OK"
- Open services.msc (Start > Run > services.msc)
- Restart the SQL Server (ION) service. Depending on the severity of the occurrence the server may need to be rebooted to release the RAM being used.
Released for:Schneider Electric Global