{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What size wrench is needed to remove the NetShelter pallet bracket?
Issue:
Customer may ask what size the pallet bracket bolts are.

Product Line:
NetShelter SX, NetShelter SV, NetShelter VX

Environment:
All versions and serial ranges.

Cause:
Customer wants to make sure they have the proper tools on hand.

Resolution:
NetShelter SX, SV and VX pallet brackets require a 13 mm wrench.
The NetShelter SV also requires a T30 Torx wrench (included). If the bolts are too tight for the included T30 Torx tool please use a T30 Torx socket and socket wrench.

Schneider Electric Global