I have a new Magelis BOX PC and the UPS/backup battery alarm is ON. I do not have the battery, how to I disable the alarm?
Published date:
28 January 2019
Issue:
I have a new Magelis BOX PC and the UPS/backup battery alarm is ON. I do not have the battery, how to I disable the alarm?
Product Line:
Magelis BOX PC
Environment:
Cause:
Resolution:
Go to Control Panel > System Monitor > Properties > Battery.
Change the settings to disable the buzzer first, check apply.
Then disable the battery function to get rid of the dialog box, check apply.
(If it is not done in this order the buzzer may stay on).
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.