The processor derives its default IP address from its factory-assigned MAC address. The MAC address for the processor is displayed on the front of the module. The default address is in the format 10.10.x.y, where x and y are derived from the last 2 octets of the MAC address. To determine the default IP address of a module, follow these steps..

NOTE: There are many resources for converting hex numbers to decimal numbers. For example,
you can use the Windows calculator in scientific mode.
NOTE: There are many resources for converting hex numbers to decimal numbers. For example,
you can use the Windows calculator in scientific mode.
Released for:Schneider Electric Global