{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is the VW3A1101 keypad compatible with the ATV600 and ATV900 Series Process Drives?

Article available in these languages: Spanish

Issue:
VW3A1101 compatibility with the ATV600 and ATV900 Drives

Product Line:
ATV600 and ATV900 series

Environment:
All models, All serial numbers

Cause:
Information not available in current literature.

Resolution:
The VW3A1101 keypad is not compatible with the Altivar Process Drives. It is only compatible with ATV61, ATV71, ATV212, ATV312, and ATV32 Series Drives.

The keypad part number for ATV630 & ATV930 process drive is VW3A1111. An optional door mounting kit part number is VW3A1112.

Schneider Electric Global