{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: Why won't the ATV630 drive run in reverse?

Article available in these languages: Finnish

Issue:
ATV630 won't operate in reverse.

Product line:
ATV600, ATV630, ATV650, Altivar Process

Environment:
All

Cause:
Configuring Reverse Motor Operation on Altivar 630 Process Drives

Resolution:
The Factory settings for the Process Drive to run in reverse is not allowed.
To allow Reverse operations:
Go to Complete Settings > Command and Reference > Reverse Disable, change the setting from Yes (meaning Reverse is not allowed) to No (meaning Reverse is allowed) and save.  Now, you should be able to operate the drive in Reverse.

Schneider Electric Global