Issue:
Maximum input voltage range of the ATV6XX "N4".
Product Line:
Altivar 6XX process drive family
Environment:
All models, All serial numbers.
Cause:
N/A
Resolution:
The range of the input voltage for the ATV6XX Process drive family is 380 - 15% to 480 +10% or a range of 323 to 528VAC, three phase.
Maximum input voltage range of the ATV6XX "N4".
Product Line:
Altivar 6XX process drive family
Environment:
All models, All serial numbers.
Cause:
N/A
Resolution:
The range of the input voltage for the ATV6XX Process drive family is 380 - 15% to 480 +10% or a range of 323 to 528VAC, three phase.
Released for:Schneider Electric Global