Issue:
Adjust the units in the ATV Process drive.
Product Line:
Altivar Process
ATV6xx
ATV9xx
Environment:
All part numbers
Cause:
Default units (Pressure in Bar, Flow in M3/h. Temp in deg C, Currency in Euro) may not be applicable to all customers in all regions of the world.
Resolution:
Using the HMI:
Under Menu 5 :[Complete settings], and subMenu 5.3 [Define system units] these settings can be manually changed.
To change using SoMove - See attached PDF.
Adjust the units in the ATV Process drive.
Product Line:
Altivar Process
ATV6xx
ATV9xx
Environment:
All part numbers
Cause:
Default units (Pressure in Bar, Flow in M3/h. Temp in deg C, Currency in Euro) may not be applicable to all customers in all regions of the world.
Resolution:
Using the HMI:
Under Menu 5 :[Complete settings], and subMenu 5.3 [Define system units] these settings can be manually changed.
To change using SoMove - See attached PDF.
Released for:Schneider Electric Global