Issue:
ATV630 process drive set up for anti jam.
Product Line:
Altivar ATV630 ATV660 process drives
Environment:
All
Cause:
Anti Jam function Programming
Resolution:
Yes, the ATV630's Anti Jam function allows the pump to execute forward, and then reverse pump rotation cycles. See the attached file for programming assistance.
ATV630 process drive set up for anti jam.
Product Line:
Altivar ATV630 ATV660 process drives
Environment:
All
Cause:
Anti Jam function Programming
Resolution:
Yes, the ATV630's Anti Jam function allows the pump to execute forward, and then reverse pump rotation cycles. See the attached file for programming assistance.
Released for:Schneider Electric Global