Resolution:
The ATV630 drive comes with three analog inputs. Each is programmable to be used for voltage or current.
The Min and Max Values are independently adjustable to allow setting up as voltage or current speed reference for most applications. For example, 0-10V, 2-10V, 4-20mA, 20-0mA, etc.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.