Issue:
Wants to setup an ATV630 Process drive to follow AI2 (Analog Input 2), instead of AI1 as reference.
Product Line:
ATV630, Altivar Process
Resolution:
From the Main Menu:
Wants to setup an ATV630 Process drive to follow AI2 (Analog Input 2), instead of AI1 as reference.
Product Line:
ATV630, Altivar Process
Resolution:
From the Main Menu:
- Scroll down and select menu 5 Complete Settings
- Scroll down and select menu 5.5 Command and Reference
- Select Ref Freq 1 Config and assign it to AI2
- Unless an HOA (Hand Off Auto) function is used, set Ref 1B switching to [Ref Freq channel 1]
- Also set Freq Switch Assign to [Ref Freq Channel 1].
Released for:Schneider Electric Global